Lubrication-free without contamination: Bearing technology for labelling machines

Dry-operating high-performance polymers in format adjustment of Krones labelling systems

Up to 50,000 containers per hour can be labelled with just one unit – this number alone says enough about the newly developed Sleevematic TS from Krones AG. The company has succeeded in doubling the performance of the system compared to the predecessor series. One major reason for this is that instead of the classic cutting of the sleeves they are now micro-perforated. A large number of lubrication-free plain bearing components from igus®, which have proven their worth at Krones for many years, are also used.

Profile

Our products are used in the "Sleevematic TS" machine from Krones.

Problem

Krones AG manufactures and sells machinery, plants and systems primarily for the beverage and liquid food industry and considers itself to be a systems provider rather than a pure machine supplier. The turn-key systems cover all processes, from beverage production, packaging and labelling through to inspections and palletisation. There are various methods for labelling; one of those used by Krones is the stretch or shrink technology of the Sleevematic series.
 
Here, Krones now offers an advanced technology with the Sleevematic TS. The TS stands for Top Speed, because with it, it is possible to label up to 50,000 containers per hour with just one unit. Before the individual sleeves are applied to (shot onto) the bottles, cans or other containers, they are no longer cut individually from the roll, but the sleeve is now micro-perforated. It is thus possible to allow continuous movement of the sleeves. Instead of cutting blades, the Sleevematic TS uses two rotating perforation cutters. In addition to the increased output, a further advantage is the significantly longer service life of the cutters. While the four cutting blades required in the past can be used for approximately five million cuts, the present two perforation knives are designed for up to 70 million cuts.
 
Rotary and linear bearing solutions are used at the various stations of the labeller.
Since highest safety standards for the protection of consumers are applicable to beverage and food technology, it is important for designers to be able to rely on products that do not require external lubrication, thus eliminating the possibility of contamination of the food or beverage.
 
Based on the modular concept of Krones, the Sleevematic TS also made use of existing components. The company continues to rely on our lubrication-free plastic solutions for various adjustable parts and other movable components.

Solution

Transverse and height adjustment of belt station (Picture 1 below):
The transverse adjustment of the belt station is ensured by an iglidur J trapezoidal thread flange nut, which is insensitive to dirt and lubrication-free. For the height adjustment, iglidur J flange nuts and FJUMT adapters are used for easy installation in combination with the sheet metal bending parts.
 
Height adjustment of the sleeve brush (Picture 2):
The height adjustment of the sleeve brush is ensured by a trapezoidal lead screw nut in combination with drylin R solid plastic plain bearings. This made it possible to work very compactly and cost-effectively.
 
Transverse and height adjustment of pre-shrink unit (pictures 3 and 4):
The height adjustment of the pre-shrink unit was implemented with a drylin SLW-1040 lead screw module including clamping, position indicator and crank for format adjustment. The compact design allows for easy integration. The transverse adjustment can also be precisely adjusted in width with a hand crank.
 
Height adjustment of the down-holder (picture 5):
A lead screw module of the type SLW-2080 is used in the height adjustment of the down-holder. It enables a simple and user-friendly operation of the machine. In addition, plastic energy chains undertake the guidance of the cables.
 
Adjustment of inlet and outlet sensor (pictures 6 and 7):
Both the inlet and outlet sensors are adjusted with a WS-1040 profile rail and a carriage including a manual clamp. By the individual weighing, the adjustment could be made very compact and flexible.
 
Height adjustment of guide roller (picture 8):
A drylin SLW-1040 lead screw module including angle drive and accessories is used for the height adjustment of the guide pulley. It was possible to make the compact adjustment unit more user-friendly by deploying the angular drive. The adjustable roller determines the position of the additional perforation on the label.
 
Film accumulator with guide rollers (picture 8):
Previously used metal bearings in the guide rollers did not run easily enough and the complete roller partially stopped. Today, they each consist of two smooth-running xiros polymer ball bearings and an anodised aluminium tube. Depending on the size of the system, up to 36 guide rollers are used. The xirodur high-performance plastic in the ball bearings also enables very good coefficients of friction and wear.
 
Adjustment of the safety door (picture 9):
Finally, the adjustment of the safety door is ensured via the drylin N-27 series. The extremely flat guidance could be accommodated in a narrow space and secured with the Plexiglas protection door in front of the access into the perforation.

"We are dependent on partnerships [...] but it must be something more than the pure product. Therefore, it is also very important to us that our suppliers not only offer good products, but also complete assemblies or systems. And this also works very well with igus."
 
Josef Mayer, Head of Product Management Inspection and Labelling Technology at Krones AG
Transverse adjustment and height adjustment of belt station iglidur J Picture 1: Left: Transverse adjustment of belt station with iglidur J trapezoidal thread flange nut. Right: Height adjustment of belt station with iglidur J flange nuts and FJUMT adapters.
Height adjustment of sleeve brush with trapezoidal lead screw nut and RJMP solid plastic bearing Picture 2: Height adjustment of sleeve brush with trapezoidal lead screw nut and RJMP solid plastic bearing.
Transverse adjustment of pre-shrink unit Bild 3: Transverse adjustment of pre-shrink unit: the desired width can be adjusted by hand wheel.
Height adjustment of pre-shrink unit with drylin SLW-1040 Picture 4: Height adjustment of the pre-shrink unit with drylin SLW-1040 complete solution including clamping, position indicator and crank for the format adjustment of the bottle types.
Height adjustment of hold-down device with SLW-2080 Picture 5: Height adjustment of hold-down device with SLW-2080 special solution. The energy chains undertake the guidance of the cables.
Adjustment of inlet sensor with WS-1040 profile rail and carriage Picture 6: Adjustment of the inlet sensor by means of a WS-1040 profile rail and a carriage including manual clamp.
Adjustment of outlet sensor by drylin WS-1040 profile rail and carriage Picture 7: Adjustment of outlet sensor by means of a drylin WS-1040 profile rail and a carriage including manual clamp.
Height adjustment of guide roller with drylin SLW-1040 lead screw module Picture 8: Height adjustment of guide roller with a drylin SLW-1040 lead screw module including angular drive and accessories. Depending on the size, between twelve and 36 guide rollers with two xiros ball bearings each are used in the film accumulator.
Adjustable protection door with drylin N-27 Picture 9: Adjustable protection door through the drylin N-27 type series.

Krones AG was founded in 1951 and is headquartered in Neutraubling near Regensburg. The company manufactures and sells machinery, plants and systems primarily for the beverage and liquid food industry and considers itself to be a systems provider rather than a pure machine supplier. "We offer our customers turn-key systems that are tailored to their needs," explains Josef Mayer, Head of Product Management Inspection and Labelling Technology at Krones. "This covers all processes, from beverage production, packaging and labelling through to inspections and palletisation. "There are various methods for labelling; one of those used by Krones is the stretch or shrink technology of the Sleevematic series.
Sleevematic TS labelling machines The Sleevematic TS labelling machine from Krones AG can label up to 50,000 containers per hour with just one unit.
igus® products are used in the "Sleevematic TS" machine from Krones.

Here, you can find the products used

Here you can find further interesting applications from very different areas of use:


ที่ปรึกษาและการสนับสนุน

เรายินดีให้คำปรึกษากับคุณ

Photo
Aw Kai Hua

Product Manager iglidur® bearings ASEAN

เขียนอีเมล

จัดส่งและให้คำปรึกษา

ในบุคคล:

วันจันทร์ถึงวันศุกร์ตั้งแต่เวลา 8.30 น. - 5.30 น.

Online:

วันจันทร์ถึงวันศุกร์ตั้งแต่เวลา 8.30 น. - 5.30 น.


เงื่อนไข "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "รางสำหรับเครน", "ConProtect", "cradle-chain", " ;CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "รางแบบง่าย", "e-chain®", " ระบบ e-chain® ", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", " ระบบ energy chain ", "Enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear" , "iglidur", "igubal", "igumid", "igus", "igus พัฒนาการเคลื่อนที่", "igus:bike", "igusGO", "igutex", "iguverse" , "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "พลาสติกเพื่ออายุการใช้งานที่ยาวนานขึ้น", "print2mold" , "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe" , "speedigus", "superwise", "ใช้งานแบบแห้ง", "tribofilament", "triflex", "twisterchain", "เมื่อมันเคลื่อนที่ igus จะพัฒนา", "xirodur", " Xiros " และ "ใช่" เป็นเครื่องหมายการค้าที่ได้รับการคุ้มครองตามกฎหมายของ igus® GmbH/ Cologne ในสหพันธ์สาธารณรัฐเยอรมนี และในกรณีที่มีผลบังคับใช้ในต่างประเทศบางประเทศ นี่เป็นรายการเครื่องหมายการค้าโดยย่อ (เช่น อยู่ระหว่างดำเนินการยื่นขอเครื่องหมายการค้าหรือเครื่องหมายการค้าจดทะเบียน) ของ igus® GmbH หรือบริษัทในเครือของ igus® ในเยอรมนี สหภาพยุโรป สหรัฐอเมริกา และ/หรือประเทศหรือเขตอำนาจศาลอื่นๆ

igus® GmbH ไม่ได้จำหน่ายผลิตภัณฑ์ใดๆ ของบริษัท Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber และผู้ผลิตไดร์ฟอื่น ๆ ทั้งหมดที่ระบุไว้ในเว็บไซต์นี้ ผลิตภัณฑ์ที่นำเสนอโดย igus® เป็นของบริษัท igus® GmbH