Lightweight and durable even when fully loaded

Robust joint and plain bearings in the
heavy-duty e-cargo bike


To improve air quality in cities and avoid gridlock, more and more logistics companies are bringing packages to people's doorsteps on electric cargo bikes. However, in order to be able to exist as a sensible supplement to lorries in the long term, e-cargo bikes must be one thing above all: robust and low-maintenance. The designers from b&p engineering therefore rely on plastic bearings from igus in their heavy-duty model.

Profile

  • What was needed: Alternative for metallic bearings in the steering and trailer coupling
  • Requirements: Durable, corrosion-free, resistant to UV radiation, dirt and temperature fluctuations, self-adjusting, lubrication-free and maintenance-free, lightweight
  • Application area: Bicycle industry
With the booming of online retail sales, the number of vehicles have increased on the roads in cities, causing traffic congestion and poor air quality. CEP service providers are therefore looking for cleaner transport solutions such as emission-free lorries or electric cargo bikes. One of the manufacturers of such e-cargo bikes is the b&p engineering mobility GmbH from Scheßlitz near Bamberg. Their innovative, four-wheeled heavy-duty model is a true Hercules among cargo bikes. Logistics specialists can use it to transport parcels weighing up to 250 kilograms to house doors. Hermes is currently testing the bikes in Stuttgart, while GLS is already using them in Nuremberg.
E-cargo bikes from p&p The heavy-duty e-cargo bike from b&p is capable of carrying loads of up to 250 kilograms. GLS already uses them in Nuremberg.

Problem

E-cargo bikes form an extremely competitive growth market that more and more start-ups are jumping into. "We can only survive in this strong competition if we continuously work out innovative solutions," says Wolfgang Hindel, Sales Director e-mobility at b&p. A high payload alone is not enough. To deliver as efficiently as possible, logistics operators want e-cargo bikes that are manoeuvrable yet highly reliable and low-maintenance. "We therefore designed our vehicle to be easy to manoeuvre and steer, and to withstand around 6,000 kilometres between service intervals. That is above average in our industry." To achieve this, the designers have thought along new lines. Many parts do not originate from classic bicycle construction, but are borrowed from the e-scooter sector and the motorcycle sector - including brakes, wheels and chains.
It was also necessary to rethink the steering rod bearing and find an alternative to classic rolling or plain bearings made of metal. These were out of the question for several reasons: first, due to edge loads there would be a constant risk of premature failure. Second, installation would be comparatively complicated: "We would have had to use additional encapsulation and sealing of the metal bearings to protect them from corrosion due to wind and weather," says Vincent Okroy, the vehicle's designer. And third, retrofits and readjustments would be necessary to compensate for misalignments - an expense that they wanted to avoid. At the same time, b&p was fundamentally committed to saving as much weight as possible in all components. 

Solution

With components from igus, several birds could be killed with one stone. The engineers chose a hard-anodised, coated igus aluminium hollow shaft as the steering rod, which is actually used for linear guides in mechanical engineering. It is mounted on an igubal spherical bearing of the series EGLM-30-LC. In it, the steering rod can move linearly and move down and up at the same time, and the front cross member can thus pivot around the frame. For example, a bike can ride on the curb without the frame twisting. Exact alignment of the bearing housing is not necessary because the bearing automatically compensates for misalignments and edge loads. It operates reliably at temperatures from -30°C to +80°C and is resistant to moisture, UV light and salt. It doesn't need packaging and seals that protect it from corrosion.
The spherical ball made of iglidur W300 material operates completely lubrication-free at lowest coefficients of friction. The bearing housing, made of igumid G polymer, is extremely robust: it withstands a static axial load of 4,000N for a short time and a radial load of 17,000N. "A good plastic bearing can withstand what a steel bearing can," Okroy says. This is not only proven by tests in the igus test laboratory. "The bearings are strong and up to all everyday biking situations, even with a full load of 250 kilograms. This has also been proven by our trial tests, in which the vehicle covered 80,000km with a full load." Last but not least, the igubal bearing scores with its low weight of only 26 grams. Comparable metal spherical plain bearings including enclosures and sealing, on the other hand, weigh around 120 grams.

The weight advantage is also used by b&p on the rotatable head of the attachable trailer coupling: iglidur X bushings with very high compressive strength are used here. 

"The polymer bearings from igus are inconspicuous at first glance. But they have helped us save weight, reduce assembly time and increase the robustness of the vehicle while reducing maintenance."

 

Vincent Okroy, designer of the Heavy Duty cargo bike

Steering bearing in b&p cargo bike Dry-operating igubal spherical bearings in the steering contribute to a higher durability of the e-cargo bike and reduce the maintenance.
Heavy duty e-cargo bike from b&p Innovative: Many components come from the e-scooter and motorcycle sector.

Further information

iglidur plain bearing product variety

iglidur plain bearings

Materials, standard product range, special parts ... everything you need to know about our plain bearings
Discover now
Various igubal bearings

igubal spherical bearings

Spherical and pillow block bearings, clevises, fixed flange bearings ... the wide variety of self-aligning bearings
Discover now
Cargo bike

Products for cargo bikes

Robust bearings for handlebar, box flap, stand and more
Discover now


เงื่อนไข "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "รางสำหรับเครน", "ConProtect", "cradle-chain", " ;CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "รางแบบง่าย", "e-chain®", " ระบบ e-chain® ", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", " ระบบ energy chain ", "Enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear" , "iglidur", "igubal", "igumid", "igus", "igus พัฒนาการเคลื่อนที่", "igus:bike", "igusGO", "igutex", "iguverse" , "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "พลาสติกเพื่ออายุการใช้งานที่ยาวนานขึ้น", "print2mold" , "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe" , "speedigus", "superwise", "ใช้งานแบบแห้ง", "tribofilament", "tribotape", "triflex", "twisterchain", "เมื่อมันเคลื่อนที่ igus จะพัฒนา", "xirodur", " Xiros " และ "ใช่" เป็นเครื่องหมายการค้าที่ได้รับการคุ้มครองตามกฎหมายของ igus® GmbH/ Cologne ในสหพันธ์สาธารณรัฐเยอรมนี และในกรณีที่มีผลบังคับใช้ในต่างประเทศบางประเทศ นี่เป็นรายการเครื่องหมายการค้าโดยย่อ (เช่น อยู่ระหว่างดำเนินการยื่นขอเครื่องหมายการค้าหรือเครื่องหมายการค้าจดทะเบียน) ของ igus® GmbH หรือบริษัทในเครือของ igus® ในเยอรมนี สหภาพยุโรป สหรัฐอเมริกา และ/หรือประเทศหรือเขตอำนาจศาลอื่นๆ

igus® GmbH ไม่ได้จำหน่ายผลิตภัณฑ์ใดๆ ของบริษัท Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber และผู้ผลิตไดร์ฟอื่น ๆ ทั้งหมดที่ระบุไว้ในเว็บไซต์นี้ ผลิตภัณฑ์ที่นำเสนอโดย igus® เป็นของบริษัท igus® GmbH