Extra-strong plain bearings in oscillating axle for semi-trailers

Maintenance-free, lubrication-free bearing points thanks to iglidur and igutex plain bearings

Profile

What was needed: 
Plain bearings with and without flange, thrust washers

Requirements:
Highly resilient, weather-resistant, lubrication-free / as little maintenance as possible

Industry: 
Commercial vehicles

Success for the customer: 
Lubrication-free bearing points that make maintenance easier for the end customer.
Oscillating axle for semi-trailers

Problem:

Bronze bearings were initially to be used in the oscillating axles of the semi-trailer. However, as these require additional lubricants, maintenance and servicing would have become very time-consuming. 

Solution:

The use of iglidur G plain bearings and thrust washers made of the heavy-duty material igutex TX1 made the use of additional lubricants superfluous and thus reduced maintenance and servicing to a minimum.

Excavator with pulley module

Working at a depth of 65 metres

One product Demarko develops is an oscillating axle for an articulated lorry trailer. Bearing point lubrication poses a particular challenge. A central lubrication system would increase production costs. So the design engineers were looking for an alternative that requires no additional lubricants. Now they use lubrication- and maintenance-free iglidur G plain bearings and igutex TX1 thrust washers.

Articulated trailers are used to transport oversized and particularly heavy objects. Trailer design and function ensure uniform wheel pressure distribution on the road surface, regardless of bumps. But they are not in continuous use like ordinary cargo trailers. For instance, they are sometimes exposed to the weather for months without the bearing points being moved or lubricated. Lubricated bearings would make the maintenance and repair of all bearing points in the oscillating axles cumbersome and time-consuming and therefore unattractive for the end customer. So Demarko was looking for a lubrication-free alternative.

Used in underground railway construction

The excavator with pulley module is used, for example, in the construction of underground railway lines that pass underneath the already existing underground railway network. It is therefore used in urban areas and must therefore be as compact and easy to transport as possible. In fact, the dimensions in the transport position with the hose reels folded in are identical to those of the conventional excavator.
 
With its grab, the excavator can move large quantities of earth out of the underground tunnels and load a whole 5 tons of material in one swoop. Loads and forces acting on the machine are thus considerable. Added to this are the weather, strong vibrations and dust. The operating conditions for all components are therefore demanding.


เงื่อนไข "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "รางสำหรับเครน", "ConProtect", "cradle-chain", " ;CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "รางแบบง่าย", "e-chain®", " ระบบ e-chain® ", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", " ระบบ energy chain ", "Enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear" , "iglidur", "igubal", "igumid", "igus", "igus พัฒนาการเคลื่อนที่", "igus:bike", "igusGO", "igutex", "iguverse" , "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "พลาสติกเพื่ออายุการใช้งานที่ยาวนานขึ้น", "print2mold" , "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe" , "speedigus", "superwise", "ใช้งานแบบแห้ง", "tribofilament", "tribotape", "triflex", "twisterchain", "เมื่อมันเคลื่อนที่ igus จะพัฒนา", "xirodur", " Xiros " และ "ใช่" เป็นเครื่องหมายการค้าที่ได้รับการคุ้มครองตามกฎหมายของ igus® GmbH/ Cologne ในสหพันธ์สาธารณรัฐเยอรมนี และในกรณีที่มีผลบังคับใช้ในต่างประเทศบางประเทศ นี่เป็นรายการเครื่องหมายการค้าโดยย่อ (เช่น อยู่ระหว่างดำเนินการยื่นขอเครื่องหมายการค้าหรือเครื่องหมายการค้าจดทะเบียน) ของ igus® GmbH หรือบริษัทในเครือของ igus® ในเยอรมนี สหภาพยุโรป สหรัฐอเมริกา และ/หรือประเทศหรือเขตอำนาจศาลอื่นๆ

igus® GmbH ไม่ได้จำหน่ายผลิตภัณฑ์ใดๆ ของบริษัท Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber และผู้ผลิตไดร์ฟอื่น ๆ ทั้งหมดที่ระบุไว้ในเว็บไซต์นี้ ผลิตภัณฑ์ที่นำเสนอโดย igus® เป็นของบริษัท igus® GmbH