iglidur® H - Material data

Materials table

General featuresUnitiglidur® Htest method
Densityg/cm³1,71 
Colour Gray 
Max. humidity absorption at 23°C/50% R. H.% weight0,1DIN 53495
Max. water absorption% weight0,3 
Coefficient of surface friction, dynamic, against steelµ0,07 - 0,2 
PV values max. (dry)MPa x m/s1,37 

Mechanical properties
Bending E-moduleMPa12.500DIN 53457
Tensile strength at +20 °CMPa175DIN 53452
compressive strengthMPa81 
Maximum recommended surface pressure (20° C)MPa90 
Shore D hardness 87DIN 53505

Physical and thermal properties
Max. long term application temperature°C+200 
Max. short term application temperature°C+240 
Lower application temperature°C-40 
Heat conductivity[W/m x K]0,6ASTM C 177
Coefficient of thermal expansion (at 23° C)[K-1 x 10-5]4DIN 53752

Electrical properties1)
Specific forward resistanceΩcm< 105DIN IEC 93
Surface resistanceΩ< 102DIN 53482
1) The good conductivity of this plastic can under certain conditions promote corrosion on a metallic contact body.
'Table 01: Material Data

pv-values H
 

Fig. 01: Permitted PV values for iglidur®{SBA} bearings with 1 mm wall thickness in dry operation against a steel shaft, at 20°C, installed in a steel housing.
 
X = gliding speed [m/s]
Y = load [MPa]

 
iglidur® H is a fiber-reinforced thermoplastic material especially developed for applications in high atmospheric humidity or under water. Bearings made of iglidur® H can be used completely free of lubrication; in application in the wet area, the surrounding media acts as additional lubricant.

Figure 02: Maximum recommended surface pressure dependent on the temperature (90 MPa to +20 °C)

X = Temperature [°C]
Y = Load [MPa]
Figure 03: Deformation under load and temperatures

X = Load [MPa]
Y = Deformation [m/s]

Mechanical properties

Maximum recommended surface pressure represents a mechanical material parameter. Tribological conclusions cannot be drawn from it. With increasing temperatures, the compressive strength of iglidur® H plain bearings decreases. Fig. 02 clarifies this connection.
 
Figure 03 shows the elastic deformation of iglidur® H with radial loads. Under the maximum recommended surface pressure of 90 MPa, the deformation amounts to about 2.5%.

Maximum surface speed

m/s Rotary oscillating Linear
Constant 1 0,7 3
Short-term 1,5 1,1 4
Table 02: Maximum surface speeds

Permitted surface speeds

The maximum permitted surface speed is dependent on whether the temperature in the bearing location rises strongly or not. iglidur® H is suited in dry operation for a maximum surface speed of 1 m/s (rotating) and 4 m/s (linear) respectively. Linear movements enable higher surface speeds, as a large area of the shaft contributes to the cooling.

iglidur® H Operating temperature
Lower - 40 °C
Upper, long-term + 200 °C
Upper, short-term + 240 °C
Secure axially in addition + 120 °C
Table 03: Temperature limits for iglidur® H

Temperatures

With increasing temperatures, the compressive strength of iglidur® H plain bearings decreases. Fig. 02 clarifies this connection.
 
The temperatures prevailing in the bearing system also have an influence on the bearing wear. An additional securing is recommended at temperatures higher than +120°C.

Figure 04: Coefficients of friction dependent on the surface speed, p = 0,75 MPa

X = Surface speed [m/s]
Y = Coefficient of friction μ
Figure 05: Coefficients of friction dependent on the load, v = 0,01 m/s

X = Load [MPa]
Y = Coefficient of friction μ

Friction and wear

The coefficient of friction alters like the wear resistance with increasing load.
Interestingly, the friction coefficient µ lowers slightly with the increase of surface speed at constant load (see Figures. 04 and 05)
iglidur® H Dry Grease Oil Water
Coefficients of friction µ 0,07 - 0,2 0,09 0,04 0,04

Table 04: Coefficients of friction for iglidur® G against steel
(Ra = 1 µm, 50 HRC)

Fig. 06: Wear, rotating application with various Figure 06: Wear, rotating application with different shaft materials, p = 1 MPa, v = 0,3 m/s
 
X = shaft materials
Y = wear [μm/km]
 
A = Aluminum, hard-anodized
B = machining steel
C = Cf53
D = Cf53, hard chrome-plated
E = St37
F = V2A
G = X90

Shaft materials

The Fig. 06 and 07 display the results of tests with different shaft materials conducted with plain bearings made of iglidur® H.
 
Bearings made of iglidur® H display a distinctly different behaviour with different shaft materials in rotating and swivelling applications. While the Cf53 and St37 shafts feature the best coefficients of wear in rotating applications, the V2A shaft that figures way below in rotating movements is, besides the St37, the most suited for pivoting movements. In contrast, hard-chromed shafts with iglidur® H bearings have advantage only with very low loads.
Fig. 07: Wear in oscillating and rotating Fig. 07: Wear in pivoting and rotating applications with various shaft materials, p = 2 MPa
 
Y = wear [μm/km]
 
A= Cf53
B= hard chrome-plated
C= V2A
D= St37
 
Blue = rotating
Pink = oscillating

Medium Resistance
Alcohols +
Hydrocarbons +
Greases, oils without additives +
Fuels +
Diluted acids + to 0
Strong acids + to -
Diluted bases +
Strong bases +
+ resistant      0 limited resistance      - not resistant
All specifications at room temperature[+20 °C]
Table 05: Chemical resistance of the iglidur® bearings H


Electrical properties

Specific forward resistance < 105 Ωcm
Surface resistance < 102 Ω
iglidur® H bearings are electrically insulating.

Chemical resistance

iglidur® H bearings have a good resistance against chemicals. Hence even an aggressive chemical can act as lubricant.

The iglidur® H bearings cannot withstand hot, oxidizing acids.

Radioactive rays

iglidur® H withstands both the neutron and gamma particle radiations without noticeable loss to its excellent mechanical properties. iglidur® H bearings are radiation resistant up to a radioactive intensity of 2 x 10² Gy.

UV-resistant

iglidur® H bearings are only conditionally resistant to UV rays. Under the influence of weathering, the surface of iglidur® H becomes harsher, and the compressive strength of the material drops.

Vacuum

Note that for use in vacuum, water elements, even if only little, should be degassed.

Electrical properties

iglidur® H bearings are electrically conductive.

Maximum moisture absorption
by +23 °C/50 % r. F. 0,1 weight-%
Max. water absorption 0,3 weight-%
Table 06: Humidity absorption of iglidur® H
Effect of moisture absorption on plain bearings Diagram 10: Effect of moisture absorption
 
X = Moisture absorption [weight %]
Y = Reduction of inside diameter [%]

humidity absorption / moisture absorption

The humidity absorption of iglidur® H bearings is about 0.1% in standard climatic conditions. The saturation limit in water is 0,3 %. iglidur® H does not soak and is therefore very well suited for application in wet environment.

Diameter
d1 [mm]
Shaft h9
[mm]
iglidur® H
F10 [mm]
Housing H7
[mm]
Up to 3 0 - 0,025 +0,006 +0,046 0 +0,010
> 3 to 6 0 - 0,030 +0,010 +0,058 0 +0,012
> 6 to 10 0 - 0,036 +0,013 +0,071 0 +0,015
> 10 to 18 0 - 0,043 +0,016 +0,086 0 +0,018
> 18 to 30 0 - 0,052 +0,020 +0,104 0 +0,021
> 30 to 50 0 - 0,062 +0,025 +0,125 0 +0,025
> 50 to 80 0 - 0,074 +0,030 +0,150 0 +0,030

Table 07: Important tolerances for iglidur® H bearings according to ISO 3547-1 after the press-fit.

Installation tolerances

iglidur® H bearings are standard bearings for shafts with h-tolerance (recommended minimum h9). The bearings are designed for press-fit in a housing with h7 tolerance. After the installation in a housing with nominal diameter, the inner diameter of the bearing automatically adjusts to the F10 tolerance. In certain dimensions the tolerance in dependence on the wall thickness deviates from this (See delivery program )

ที่ปรึกษาและการสนับสนุน

เรายินดีให้คำปรึกษากับคุณ

Photo
Aw Kai Hua

Product Manager iglidur® bearings ASEAN

เขียนอีเมล

จัดส่งและให้คำปรึกษา

ในบุคคล:

วันจันทร์ถึงวันศุกร์ตั้งแต่เวลา 8.30 น. - 5.30 น.

Online:

วันจันทร์ถึงวันศุกร์ตั้งแต่เวลา 8.30 น. - 5.30 น.


เงื่อนไข "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "รางสำหรับเครน", "ConProtect", "cradle-chain", " ;CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "รางแบบง่าย", "e-chain®", " ระบบ e-chain® ", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", " ระบบ energy chain ", "Enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear" , "iglidur", "igubal", "igumid", "igus", "igus พัฒนาการเคลื่อนที่", "igus:bike", "igusGO", "igutex", "iguverse" , "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "พลาสติกเพื่ออายุการใช้งานที่ยาวนานขึ้น", "print2mold" , "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe" , "speedigus", "superwise", "ใช้งานแบบแห้ง", "tribofilament", "tribotape", "triflex", "twisterchain", "เมื่อมันเคลื่อนที่ igus จะพัฒนา", "xirodur", " Xiros " และ "ใช่" เป็นเครื่องหมายการค้าที่ได้รับการคุ้มครองตามกฎหมายของ igus® GmbH/ Cologne ในสหพันธ์สาธารณรัฐเยอรมนี และในกรณีที่มีผลบังคับใช้ในต่างประเทศบางประเทศ นี่เป็นรายการเครื่องหมายการค้าโดยย่อ (เช่น อยู่ระหว่างดำเนินการยื่นขอเครื่องหมายการค้าหรือเครื่องหมายการค้าจดทะเบียน) ของ igus® GmbH หรือบริษัทในเครือของ igus® ในเยอรมนี สหภาพยุโรป สหรัฐอเมริกา และ/หรือประเทศหรือเขตอำนาจศาลอื่นๆ

igus® GmbH ไม่ได้จำหน่ายผลิตภัณฑ์ใดๆ ของบริษัท Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber และผู้ผลิตไดร์ฟอื่น ๆ ทั้งหมดที่ระบุไว้ในเว็บไซต์นี้ ผลิตภัณฑ์ที่นำเสนอโดย igus® เป็นของบริษัท igus® GmbH