Test reports of the motor cables

Discover all our test reports on the durability tests for our motor cables here.


Motor cable CF270.UL.25.04.D

Test number:4831
Bend radius:100mm (factor 9.1 x d)
Service life:more than 18 million strokes
In this test, the life expectancy of the CF270.UL.25.04.D was to be analysed in an e-chain with a 100mm radius.

The test showed that the expected service life of the CF270.UL.25.04.D motor cable can withstand more than 18 million strokes and can therefore be used as a reliable supply cable for motors.
Motor cable CF270.UL.D

Use of the CF270.UL.D in practice

Process automation in the automotive industry saves time and money. Automation technology is essential in the production line, where it requires a great deal of drive technology with motors and converters. From structural work to the paint shop to final assembly, systems are in different environments and come into contact with different materials. All of these areas require motor cables that meet the strict requirements of the automotive industry.

 

Download full test report

Motor cable CF38.250.04

Test number:4904
Bend radius:175mm (factor 6.5 x d)
Service life:43 million strokes
In this test, the life expectancy of the CF38.250.04 in an e-chain with a 175mm radius was to be analysed.

The test has shown that the expected service life of the CF38.250.04 motor cable can withstand 43 million strokes and therefore has large reserves. 

Use of the CF38 in practice

Cable failures are certainly never desired. However, a cable failure in crane and trolley travels is unthinkable. Reliability and maximum safety are required here. The motor cables used are therefore exposed to major challenges. Temperatures of -40°C to +80°C are not uncommon. In addition, there are usually long travels and therefore high loads due to continuous use and dust. The motor cable used must be able to withstand all these conditions.

 
Download full test report
Motor cable CF38

Motor cable CFROBOT7.25.04.C

Test number:3698
Cable typeMotor cable
Test parameter105mm/+/-180°/m
Service life:120 million cycles
This test was carried out to analyse the life expectancy of the CFROBOT7.25.04.C in a triflex.

The test result of over 12 million cycles confirms that the cable fulfils the requirements for drive technology in robotics.
Bus cable CFROBOT8

Using the CFROBOT7 in real life

The aim of the test was to determine the service life of the twistable motor cable of the CFROBOT7 robot cable family. The CFROBOT7 is required to reliably withstand continuous movement, such as in a robot with a torsion of +/-180° as it is found in the automotive industry.

In these applications, it is often the case that the robots are permanently in motion and the cables are therefore constantly exposed to this torsion. Thanks to an enclosed overall shield and the robust PUR outer jacket, this cable is ideal for movements in the 3D range.
 
Download full test report



เงื่อนไข "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "รางสำหรับเครน", "ConProtect", "cradle-chain", " ;CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "รางแบบง่าย", "e-chain®", " ระบบ e-chain® ", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", " ระบบ energy chain ", "Enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear" , "iglidur", "igubal", "igumid", "igus", "igus พัฒนาการเคลื่อนที่", "igus:bike", "igusGO", "igutex", "iguverse" , "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "พลาสติกเพื่ออายุการใช้งานที่ยาวนานขึ้น", "print2mold" , "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe" , "speedigus", "superwise", "ใช้งานแบบแห้ง", "tribofilament", "tribotape", "triflex", "twisterchain", "เมื่อมันเคลื่อนที่ igus จะพัฒนา", "xirodur", " Xiros " และ "ใช่" เป็นเครื่องหมายการค้าที่ได้รับการคุ้มครองตามกฎหมายของ igus® GmbH/ Cologne ในสหพันธ์สาธารณรัฐเยอรมนี และในกรณีที่มีผลบังคับใช้ในต่างประเทศบางประเทศ นี่เป็นรายการเครื่องหมายการค้าโดยย่อ (เช่น อยู่ระหว่างดำเนินการยื่นขอเครื่องหมายการค้าหรือเครื่องหมายการค้าจดทะเบียน) ของ igus® GmbH หรือบริษัทในเครือของ igus® ในเยอรมนี สหภาพยุโรป สหรัฐอเมริกา และ/หรือประเทศหรือเขตอำนาจศาลอื่นๆ

igus® GmbH ไม่ได้จำหน่ายผลิตภัณฑ์ใดๆ ของบริษัท Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber และผู้ผลิตไดร์ฟอื่น ๆ ทั้งหมดที่ระบุไว้ในเว็บไซต์นี้ ผลิตภัณฑ์ที่นำเสนอโดย igus® เป็นของบริษัท igus® GmbH